Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLUENRG-M2SP MAC Address issue & DTM Firmware

Hello, In one of my projects, I use BLUENRG-M2SP as a network coprocessor with a host microcontroller from STM32L0 series together. I flashed BLUENRG-M2SP with pre-compiled DTM_SPI.hex which is used by X-NUCLEO-BNRG2A1. My application code is run by ...

Blue_NRG-2 examples load but dont run

I am trying to develop some custom code using the BlueNRG-2 chip. I have my own custom board but first I am trying to get things to work on the STEVAL-BCN002V1 blue tile. That board comes preloaded with the Sensor Demo which worked fine. I am using t...

JWall.1 by Associate II
  • 885 Views
  • 0 replies
  • 0 kudos

Resolved! BALFLB-WL-08D3 with STM32WL54CC at 433MHz

Hello,i need to know if you recommend to use the BALFLB-WL-08D3 at 433MHzI design my PCB with the STM32WL54CC, and it will operate between 433MHz and 435MHz. i want to know if the BALFLB-WL-08D3 is suitable for my application or if is better to desig...

malarab by Senior II
  • 1028 Views
  • 1 replies
  • 0 kudos

BlueNRG 2

I am working with BlueNRG 2, and Tile both... I'm working in BlueNRG-1_2 DK 3.2.3. In the xx\BlueNRG-1_2 DK 3.2.3\Firmware\BLE_Examples\BLE_SerialPort\BlueNRG-2 folder, there is Server bin and hex files which work great. However, when I go to the C:\...

LPrin.1 by Associate II
  • 991 Views
  • 0 replies
  • 0 kudos

SPIRIT1 CSMA understanding problem?

Posted on August 10, 2015 at 13:32I am performing some tests on the CSMA feature. Specifically on the non persistent CCA method. I have a test process whereby every 10s the transmitting module has its TX FIFO flushed, has its FIFO filled with 20 byt...

kzkaram by Associate II
  • 2561 Views
  • 4 replies
  • 0 kudos

S2-LP medium speed data transmission example

Hello,I'm trying to find an example project where audio was streamed using the S2LP chipset, but I can only find Sigfox/LORA examples.Do you know of any off the shelf medium speed / real-time example using the S2LP IC?  Our speed requirement is aroun...

SensorTile BLE GATT Characteristic Editing

Hi,When editing the GATT characteristic in the provided software for the SensorTile, I cannot increase the size of the payload being transmitted. Even after altering the charValueLen variable, this doesn't appear to affect the length of the packet be...

byrnep8_3-1689201716475.png byrnep8_1-1689201528729.png byrnep8_2-1689201574962.png
byrnep8 by Associate
  • 784 Views
  • 0 replies
  • 0 kudos