Hello everyone. I'm facing a issue when I try to use CODED_PHY instead 1M_PHY. When I start a GAP_GENERAL_DISCOVERY_PROC, the stack returns: 0xD1 (BLE_STATUS_INVALID_SCAN_CONFIGURATION).Could anyone help me? The scan configuration is (return 0x00 - O...
Hello everyone I'm trying to use aci_gatt_clt_read_multiple_char_value() function but it are returning error 0x82 (BLE_STATUS_INVALID_PARAMS).aci_gatt_clt_read() function works as expected but I want to read multiple values for optimization purposes....
Hello thereI have a custom board based on STEVAL-IDB011V2 EVM. Is the same schematic but I have a problem with this. Apparently it boots but not run... When I flash "Hello World" example I have some issue that I can't check why.... The expected messa...
Hello there,What's the total range of BlueNRG-M2SA? I read in this forum that is 33 meters, it's correct? My application needs something about 500 meters. Does possible reach it with BlueNRG-M2SA (or BlueNRG-2)?Best Regards,Leonardo