Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WEP in AP mode

Posted on June 15, 2015 at 12:34Is there a limitation/restriction of of the WEP key lengths in AP mode?Set password to 'test1': AT+S.SCFG=wifi_wep_keys[0],7465737431 AT+S.SCFG=wifi_wep_key_lens,05 This works OK.  I can connect fine with WEP authenti...

toby by Associate II
  • 1202 Views
  • 2 replies
  • 0 kudos

STW81200 Schematic / design guidance

Posted on June 11, 2015 at 12:22I am wanting to include the STW81200 into a new product design. I am looking for the schematic for the evaluation board that I think exists, but I am not able to find it.The specific information that I am looking for ...

Create a connection between three SPWF01SA

Posted on June 10, 2015 at 08:37Hello, i want to create a connection bettween three SPWF01SA an send data via TCP - socket to any other module. Is there a possibility to create something like that. The firmware is 150410-c2e37a3-SPWF01S. Thanks and ...

menyu1 by Associate II
  • 2079 Views
  • 4 replies
  • 0 kudos

BlueNRG missing LE Advertising Report Event

Posted on June 07, 2014 at 10:48I can get two BlueNRG boards connecting, one as Peripheral and one as Central, using the code in the BLE_Chat example. In this case the Central has to know in advace the address of the Peripheral. However, when I try...

charles23 by Associate III
  • 2293 Views
  • 5 replies
  • 0 kudos

SPWF01XX Firmware Upgrade (usart)

Posted on April 25, 2015 at 07:20HelloI need to update the firmware (need the 1 command the is in release 3.3)for the above module. I have contacted the local ST agent and have received the required programs and files for the upgrade (via usart)(SPW...

Spirit1 PA Configuration

Posted on May 13, 2015 at 12:42Hi,Which PA configuration parameters should I use in order to get the maximum output power on Spirit1 and which CWC (0 - 1.2 - 2.4 - 3.6 pF) bit field should be set for 868 MHz band?According to the datasheet the max o...

hacer by Associate II
  • 1446 Views
  • 1 replies
  • 0 kudos

details are needed for HAL_LE_TX_TEST_PACKET_NUMBER

Posted on April 17, 2015 at 22:20In AN4494, Bring up BlueNRG app note, both Chapter 8 and 9 mention thatSend a further command to determine the number of packets sent by the Tx board: HAL_LE_TX_TEST_PACKET_NUMBER What is the LE command above? Where...

hui by Associate II
  • 1192 Views
  • 1 replies
  • 0 kudos