User Activity

Posted on April 19, 2016 at 15:27Hi, I am having a problem with the HTTPDFSUPDATE failing mid download here is what I see on the console:  Image length 338827 (offset 0x00080000, block len 4096)  Write len 4096 -> 0x8B000                            ...
Posted on November 17, 2015 at 15:05Between the rev 4 & Rev 6 datasheets there seems to have been a change in the centre pad size on the recommended footprint.  It now seems to ask for 8mm max x6mm max - previously it was specified as 10mmx8mm!  I h...
Posted on August 11, 2015 at 09:26Reading the documentation, I see that in some instances the HTTP header is requied to be appending to the strat of the files to be served by the HTTP server.  However it is not too clear which files requrie this. Am...
Posted on June 15, 2015 at 12:34Is there a limitation/restriction of of the WEP key lengths in AP mode?Set password to 'test1': AT+S.SCFG=wifi_wep_keys[0],7465737431 AT+S.SCFG=wifi_wep_key_lens,05 This works OK.  I can connect fine with WEP authenti...