Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI connect to SPWF01SC

Posted on July 02, 2015 at 16:04Hi, I'd like to use the SPI connection of SPWF01SC. Could you say me please which pinout description are right? Is the the DocID025635 Rev 2 and the STEVAL-IDW001V1 with SPI description right? http://www.mikrocontrol...

christos by Associate II
  • 1096 Views
  • 3 replies
  • 0 kudos

[solved]fastest communication

Posted on April 20, 2015 at 11:29Hi,I'm trying to achieve a communication between two wifi devices through a SPWFO1SA.11 , and I want to achieve the highest possible bite rate. My questions are then:-Can I use the mentioned SPI port to perform the A...

hector by Associate II
  • 4152 Views
  • 12 replies
  • 0 kudos

SPIRIT1 stucks in READY state

Posted on June 27, 2015 at 00:17We have trouble to get the SPIRIT1 on our own board working. The very basic problem is that the chip can not be switched to any other state then ready Therefor the setup for any frequency settings are not possible. We...

ralph23 by Associate II
  • 2599 Views
  • 6 replies
  • 0 kudos

Socket response time

Posted on June 25, 2015 at 15:29Hi,I'm trying to set up a communication between two SPWF01SA.A is set as the server, B as the client. I wrote a text to send from A to B when the WIND 61 + WIND 60 are detected. If a try to do it just after the WIND 6...

hector by Associate II
  • 1184 Views
  • 3 replies
  • 0 kudos

Bluetooth scatternet

Posted on June 26, 2015 at 09:40I wish to create a bluetooth scatternet. The network consists of 15 nodes (microcontroller and bluetooth module). 3 piconets (maybe more) with 5 nodes . 1-4 nodes are connected to 5 node, 5-9 nodes are connected to th...

roomanaz by Associate
  • 985 Views
  • 0 replies
  • 0 kudos

SPIRTI1 + SKY66100-11 power consumption

Posted on April 28, 2015 at 11:13Hi, I'm testing a solution with Spirit1 + SKY66100-11 for 169MHz transmission. I have a 600mA current consumption with spirit1+sky 66100-11+TCXO. Is it normal? Where Can I found a detailed technical report of current...

mauro by Associate
  • 1689 Views
  • 5 replies
  • 0 kudos

SPIRIT1 unknown state

Posted on June 11, 2015 at 22:10Hi Gaetano, I'm currently working with the SPIRIT1 on a my own board. An external clock signal is used on XIN coming from my MCU (STM32F4) at 26 MHz. And the central frequency is set to 868.3 MHz. Sometimes, I get an ...

SPIRIT1 register DEVICE_INFO content

Posted on June 15, 2015 at 15:20Unfortunately the data sheet can be evaluated as a minimum documentation for this chip. Is there any more information available e.g. for the DEVICE_INFO register, what the content is and could be and what it is tellin...

ralph23 by Associate II
  • 576 Views
  • 1 replies
  • 0 kudos