Posted on December 07, 2015 at 19:00Hi, I use Spirit1 both with 433Mhz and 868Mhz on the same custom-designed board with stm32l1. The radio parameters are set according to the individual transceiver and the software configuration is done seperately ...
Posted on May 13, 2015 at 12:42Hi,Which PA configuration parameters should I use in order to get the maximum output power on Spirit1 and which CWC (0 - 1.2 - 2.4 - 3.6 pF) bit field should be set for 868 MHz band?According to the datasheet the max o...
Posted on March 16, 2015 at 08:21Hi,I use Spirit1 on my custom board that includes stm32l162 MCU. I am trying to work the ''BasicPktTest'' example. Actually I can view the packets are being transmitted and received between two devices. But it does n...
Posted on March 10, 2015 at 08:39Hello,I have Spirit1 IKR02v3.0 development kit. It contains an STM32L151 MCU and Spirit1 RF module. But I use Spirit1 with STM32L162RD MCU for a project. I created my own project on Keil. I ported all the spirit1 fir...
Posted on December 16, 2014 at 15:56Hi,I want to learn that how many active connections can make STLBC01 (Bluetooth low energy controller) simultaneously.Regards,Hacer
Posted on March 24, 2015 at 10:41Hi, There is a code block that reads registers of spirit1 transciever in SDK_EVAL_Spi_Driver.c. It is written below:/*** @brief Read single or multiple STS2001 register* @param cRegAddress: base register's address ...