Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

OOK - Direct Rx Through GPIO

Posted on October 29, 2015 at 09:34Hi all I'm trying to use SPIRIT1 as a simple receiver of OOK modulated signal using DIRECT RX MODE THROUGH GPIO but i'm not able to obtain a clean signal, I've always spurious commutations inside my data frame. It ...

dev by Associate
  • 1090 Views
  • 1 replies
  • 0 kudos

SPBT2632C2A.AT2 Firmware Download

Posted on November 22, 2015 at 02:22Hello, I'm trying to figure out where I can download the AT2 1.5 or 1.6 firmware for the SPBT2632C2A.AT2. Our application requires features of the new firmware and we have a bunch of assembled units with freshly o...

SSL/TLS Error: Unable to connect (-1)

Posted on November 16, 2015 at 08:58Hi, I'm trying to establish a TLS communication using the one-way authentication. I loaded into the SPWF01 the CA certificate as described in the example of the AN4683 but when I try to connect to the openssl serv...

paolo23 by Associate II
  • 2465 Views
  • 6 replies
  • 0 kudos

SPWF01SA PCB Footprint

Posted on November 17, 2015 at 15:05Between the rev 4 & Rev 6 datasheets there seems to have been a change in the centre pad size on the recommended footprint.  It now seems to ask for 8mm max x6mm max - previously it was specified as 10mmx8mm!  I h...

toby by Associate II
  • 1515 Views
  • 3 replies
  • 0 kudos

BlueNR-MS Active

Posted on November 13, 2015 at 12:50Hi all!Please, can you help me. I have next problem. In My device I use BlueNRG-MS (HSI-16MHz, LSE ext - 32.768). BlueNRG init Ok, but not available in RF.  He is active with a period of 30 seconds (name ''atn_B41...

0690X00000602dxQAA.jpg 0690X00000602e2QAA.jpg
dnedov by Associate
  • 630 Views
  • 0 replies
  • 0 kudos

VCOM project from L053 to L051

Posted on November 11, 2015 at 15:29Hello, I have a query. I have a Virtual COM demo Project by ST. It is meant for L053R6 with Blue NRG chip. Will the same work on L051R6 with the same Blue NRG chip? The UART pins seem to be the same. I changed the...

sai by Associate II
  • 960 Views
  • 2 replies
  • 0 kudos

STM32L053 half duplex mode

Posted on November 11, 2015 at 11:44Hello, I am using STM32L053R6 interfaced to Blue NRG chip. I am accessing the blue NRG through VCOM. I have connected a USB to UART converter to a PC and was trasmitting the VCOM data over this. It worked!!! Now...

sai by Associate II
  • 824 Views
  • 0 replies
  • 0 kudos

httpd_gen in linux

Posted on November 10, 2015 at 19:47Hey folks,I'm trying to to create an img file from a web page using httpd_gen.  The only version of httpd_gen I have is the source code (httpd_gen.c).  I compiled this using gcc on two different linux machines (x8...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.