Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Pairing BlueNRG with Android

Posted on May 30, 2016 at 07:10I have our BlueNRG device set up to use a fixed pin for pairing. I am able to successfully pair with Apple iOS decvices and windows phone when I enter the correct PIN when prompted by the device. However when connectin...

SPWF01S.11 server HTTP/0.9 version pages blocked iOS10

Posted on November 24, 2016 at 11:26Hello, I am using SPWF01.11 FW3.5 as webserver as described in a previous post. This webserver is made of 1 HTML Frameset (main.html) + 3 HTML frames (m.html / sm.html / data.html) to override the 4ko limitation. ...

be by Associate II
  • 1833 Views
  • 4 replies
  • 0 kudos

SPWF01S Nagle

Posted on November 23, 2016 at 15:58Hi, how can I configure/deactivate the Nagle-Algorithm in SPWF01S? Thanks! MBU

mbuczek by Associate II
  • 1454 Views
  • 5 replies
  • 0 kudos

Problem with SPBLE-RF SPI commands

Posted on November 21, 2016 at 20:59Hello everyone!I'm working with ST SPBLE-RF using the C code driver provided for BlueNRG-MS. I ported it for an ST8L151G6 microcontroller; the SPI communication works, the device answers correctly (0x02 and the R/...

SPBTLE-RF FW 7.2c

Posted on November 18, 2016 at 23:27Hi, i have a problem using SensorDemo_New of BlueNRG DK 2.0.2COPY_ENV_SENS_SERVICE_UUID(uuid); ret = aci_gatt_add_serv(UUID_TYPE_128,  uuid, PRIMARY_SERVICE, 10, &envSensServHandle);i get ERR_UNSPECIFIED_ERRORif c...

Connectiong to the iPhone hotspot

Posted on November 15, 2016 at 08:58Hi..I can easily connect the module to any APs and it works fine. But, I can not connect it to the iPhone hotpots.. does hotshots needs additional configuration.?

pouya by Associate II
  • 1965 Views
  • 5 replies
  • 0 kudos

spirit1 narrowband settings

Posted on October 21, 2016 at 14:55Hi,   I'm trying for lowest bandwidth settings for higher sensitivity. But packets wouldn't reach. Is there any problem with my settings? #define CHANNEL_SPACE               20e3 #define CHANNEL_NUMBER            ...

vamsi by Associate II
  • 960 Views
  • 1 replies
  • 0 kudos

SP1ML Source Code

Posted on November 10, 2016 at 12:03Does anyone know if ST have source code for the SP1ML modules available? or even a starting point for people wanting to develop custom firmware for the device.thanks #sp1ml-spirit1-stm32l151rb

sean23 by Associate II
  • 740 Views
  • 0 replies
  • 0 kudos