Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Removing the spwf01sx cgi files.

Posted on December 08, 2016 at 09:13Hi, I was wondering that if it is possible to delete the HTML and CGI file system from the module.?P.S: I can see from the documentation that it is possible to disable/enable the feature. My concern is to permanen...

pouya by Associate II
  • 931 Views
  • 1 replies
  • 0 kudos

idw01m1 deauthenticated

Posted on December 05, 2016 at 21:32Hello folks,while experimenting with an idw01m1 module, I am experiencing deauthentication with the message:WIND:40:WiFi Deauthentication 3With the '2015' firmware, the module was unable to reconnect until WiFi wa...

infor by Associate III
  • 836 Views
  • 1 replies
  • 0 kudos

M95512-A125 EEPROM IDLE CHECK

Posted on December 09, 2016 at 16:49Hi there! I am using M95512-A125 serial EEPROM in my automotive project. My question is, when i'm going to do some operation on the EEPROM, how do I know if it is completely IDLE? I know that bit WIP in the status...

BlueNRG Python Scriptlauncher

Posted on December 07, 2016 at 00:39Hi,Referring to this question: https://community.st.com/0D50X00009Xke8kSAB Dear customer,I'll try to give a feedback to you:•Can scripts be run in a normal Python debug environment rather than using BlueNRG_Scri...

WMbus libs

Posted on December 09, 2016 at 08:48Hi, I want to read some Wmbus frames using SPIRIT1. Do anyone happen to know where i can find those libs: wmbus_appli.c, wmbus_link.c, wmbus_phy.c. They were mentioned in one of ST pdf about Wmbus protocol: /exter...

Resolved! X-NUCLEO-IDB04A1

Posted on December 05, 2016 at 21:13shield of stm32f746g discoveryshield of the idb04a1is there a solution (difficult to unsolder the resistance: can we curve or cut the pin and stripe irq csn and clk ?)Br,Christophe#bluenrg #stm32f746g-disco

0690X00000605juQAA.png 0690X00000605jtQAA.png

Resolved! Bluenrg-ms bonding with PIN

Posted on December 06, 2016 at 15:28Hi,I'm using the Bluenrg-ms chipset with firmware version 7.1.e (0x715). Everything works fine, except from the authorization settings. Each device can connect to the BLE without any request for permissions (PIN)....