cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-SP1ML915

jeffm
Associate II
Posted on August 06, 2015 at 00:02

Reading and writing the SPIRIT1 radio registers directly, doesn't seem to work.

Here is one simple example...

AT/SR36=10

OK

AT/SR36?

36=88

AT/V reports SP1ML-915 HW:V1 FW:V0.12

Is there a more recent firmware version that addresses this?
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
jeffm
Associate II
Posted on August 06, 2015 at 00:23

Also, does anyone know if the source code for the image that's programmed on this EVAL board is published?

Nickname2185_O
Associate II
Posted on August 26, 2015 at 14:31

Hello,

The eval board does not integrate a dedicated FW but the same FW running on the SP1ML module, the eval is based on. For this reason we do not provide the related source code.

From your log, it comes out you have a board with a very old FW version inside. It is the origin of the issue you report. The current fw version is 1.03 and it is also available on the ST website. Part number: STSW-SP1ML915AT.

At/v

SP1ML-915 HW:V1 FW:V1.03

at/sr36?

36=88

at/sr36=10

OK

at/sr36?

36=10

Please refer to the UM1889 for a description of the tasks to be runned for the FW upgrade.

Do not hesitate to contact us again in case of any other issue.

With the Best Regards,

ST Support

jeffm
Associate II
Posted on February 12, 2016 at 20:32

Indeed the issue has been resolved by updating the firmware. Thanks.