User Activity

What is the simplest way to set the power amplifier?Unfortunately the APIs require involvement with the PA ramps and index configurations.void S2LPRadioSetPALeveldBm(uint8_t cIndex, int32_t lPowerdBm) void S2LPRadioSetMaxPALevel(SFunctionalState xNew...
Does anyone have any details on register settings to get the S2-LP running from XIN rather that a crystal? The documentation is a bit thin in this area.
Posted on August 06, 2015 at 00:02Reading and writing the SPIRIT1 radio registers directly, doesn't seem to work.Here is one simple example...AT/SR36=10OKAT/SR36?36=88AT/V reports SP1ML-915 HW:V1 FW:V0.12Is there a more recent firmware version that ...
Kudos given to