Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP - Nucleo project files for STM32L152RE

Posted on July 07, 2017 at 11:31Hi,I purchased the S2-LP development kit which contains 2 boards:- NUCLEO board equipped with STM32L152RE- S2-LP boardThe development kit contains though the project files for STM32L053R8Are available the project file...

STM32L4 and BlueNRG-MS causing hard fault

Posted on July 06, 2017 at 22:34Hi,   I am using an STM32L486, connected to a BlueNRG-MS via SPI.  I am trying to build a simple app that can advertise, with one service and a 6 characteristics.  I'm following the example in the programming guide, i...

WiFi Module Not Connecting

Posted on May 16, 2017 at 15:38Hi,I am using the STM32 Nucleo Expansion Board WiFi Module for a project. I followed the Quick Start Guide and tried to run the HTTP_Request example project. However, after asking for the SSID, password and encryption ...

Kyle Yu by Associate
  • 3010 Views
  • 2 replies
  • 0 kudos

LM2901 comparator with invertered inputs

Posted on July 05, 2017 at 12:10I'm using quad comparator LM2901.When i wanted to invert output i've just swaped places of + and - inputs.It worked on emulator but did not work on real circuit.What am i doing wrong?Maybe there is a better way to do ...

es131245 by Associate II
  • 609 Views
  • 0 replies
  • 0 kudos

SP1ML module very low RSSI

Posted on July 04, 2017 at 15:30Hello!For a project at work we're using SP1ML-915 modules. For testing I have one dongle made by ST and one PCB made in house with SP1ML module mounted and connected to USB.After sending random strings between the two...

tomaz by Associate
  • 594 Views
  • 0 replies
  • 0 kudos

SPWF04SA no longer communicates

Posted on July 03, 2017 at 17:35I'm using the X-NUCLEO-IDW04A1. After a restart, the module no longer communicates via serial port (UART).LED3 (Red - GPIO14) is On.The 'MicroPython_mode' (pull_up GPIO8) at reboot work fine.How can I restore the modu...

Python on SPWF04S

Posted on June 28, 2017 at 17:12Hi, I have a problem with SPWF04S.When send command 'AT+S.PYTHON' the answer is 'AT-S.ERROR:16:Cannot switch to Python shell'I tried to look something in datasheet, but nothing. I dont know how go over. Any idea?#pyth...

Replacement for BALF-NRG-01D3

Posted on July 02, 2016 at 18:18Hello,Kindly I'm asking about a replacement for BALF-NRG-01D3,I need a larger balun package/footprint to can assemble it manually to a PCB.Thanks in advance. #balf-nrg-01d3-bluenrg

moataz by Associate
  • 862 Views
  • 1 replies
  • 0 kudos