Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SP1ML xtal frequency

Posted on July 28, 2017 at 12:03What is the XTAL frequency of the spirit1 chip connected to SMPS of the SP1ML-868 module?I have the famous LOCKWON status, and I suppose the default configuration does not comply with XTAL frequency.#spirit1-sp1ml

Bluenrg-1 support advertising after connected?

Posted on July 26, 2017 at 11:35Dear All,I'm using BLUENRG-1  working on a beacon project. And the problem for me is that can bluenrg-1 advertising after connect by APP or phone?Base on BlueNRG-1_2 DK 2.5.0.As follow steps I try:1. set 'undirected s...

Mo Ran by Associate
  • 578 Views
  • 0 replies
  • 0 kudos

New to BLUENRG-1

Posted on July 13, 2017 at 12:06Hello all,I am new using the bluenrg-1, I would like to create an application to download into the ble module but not really sure from where to start, how to do it.I have done some test communicating with the ble usin...

jampino by Associate III
  • 1237 Views
  • 6 replies
  • 0 kudos

Initialize STMIPID02(MIPI CSI-2 deserializer)

Posted on April 15, 2014 at 10:42I'm using STMIPID02(MIPI/CSI-2 desrializer)I have initialized regieter of STMIPID02 by I2C.   but, It output no signal on parallel interface(Pixel interface)help me... anyone have more data for initialize of STMIPID0...

hh by Associate
  • 2610 Views
  • 5 replies
  • 0 kudos

BlueNRG-1: MCU and bluetooth peripheral

Posted on July 18, 2017 at 16:44Hello,Pretty new to this tiny jewel, I have trouble understanding how everything is architectured.When reading the ``datasheet'' (DocID028866 Rev 3), it seems [see fig.1] that the Cortex-M0 core is connected through a...

SPWF01SA LINK, ACT, and PWR LEDs

Posted on July 17, 2017 at 19:04Hi all,Following the schematics for the http://www.st.com/content/st_com/en/products/ecosystems/stm32-open-development-environment/stm32-nucleo-expansion-boards/stm32-ode-connect-hw/x-nucleo-idw01m1.html and the schem...

SPWF01SA HTTP POST problems

Posted on July 17, 2017 at 13:26Hi, I'm trying to use the SPWF01SA module (IDW01M1 expansion board) like an HTTP server to send some POST response to an iPhone app. Now I'm able to open a TCP Server on the 80 port, shutting down the HTTPD server. Bu...

SPWF04 SPI ISSUES

Posted on July 12, 2017 at 09:32We are using the SPWF04 SPI and have the following issues1) No Ack after TCP socket data packet sent:I can setup a client socket or a server socket and start streaming data but at some point the SPWF04S does not ack a...