Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPWF04SA always return ''Hardware Failure''

Posted on August 10, 2017 at 09:47Hi ST,Recently I try to enable AP or station mode on SPWF04SA wifi module,I connect it with my PC via UART and I can see some feedback on terminal on my PC.The question is, even though I can command SPWF04SA with it...

Wei Lu by Associate
  • 905 Views
  • 1 replies
  • 0 kudos

SPBT3.0DP2 automatic reset

Posted on February 01, 2018 at 19:01The SPBT3.0DP2 seems to generate its own nReset pulse ocaasionallyThe pulse is around 800usAny reason why this would occur ?The power supply is stable and the IO is 3.3V

pbayton9 by Associate III
  • 787 Views
  • 1 replies
  • 0 kudos

Read WIND messages from NUCLEO WIFI SPWFSA01

Posted on January 15, 2018 at 11:08Hi to all,I'm working on NUCLEO F411RE board with WiFi platform NUCLEO WIFI SPWFSA01; I'm using the X_NUCLEO_IDW01M1v2 mbed library to use this WiFi module. Library works perfectly but I'd like to read the WiFi 'WI...

DUrbano by Associate III
  • 874 Views
  • 1 replies
  • 0 kudos

SPBT3.0DP2 - HID (AT-Command)

Posted on July 29, 2017 at 01:38Hello,I'm using the SPBT3.0DP2-Module.I want to create a HID-Keyboard.How can I connect with the HIDConnect-Command? This would not work :(There are only this three commands for HIDConnect, HIDIntSend, HIDDisconnect ....

BlueNRG-1 supporting BLE and BL?

Posted on January 30, 2018 at 08:15Hello,We are using the STEVAL-IDB007V1 board and we want to use both BLE and BL. As i read, the BlueNRG-1 supports only BLE.Is there any other solution(other IC) to implement BLE/BL but also be able to download fir...

SProg by Associate III
  • 1345 Views
  • 5 replies
  • 0 kudos

BlueNRG-1 internal MCU and SPP

Posted on January 29, 2018 at 09:10Hello everyone.i am using the STEVAL-IDBB007V1 based on BlueNRG-1.I am interested on programming the internal MCU of BlueNRG-1 and use the BLE functionsBased on the Application Notes and examples, i understand that...

SProg by Associate III
  • 1367 Views
  • 3 replies
  • 0 kudos

Resolved! Where are Bluetooth LE library sources?

Posted on January 25, 2018 at 11:46Hi,I would like to use BlueNRG-2 in my project. I downloaded BlueNRG-1.2 DK software package. There is a lot of examples of applications. They use an archive library libbluenrg1_stack.a containing compiled Bluetoot...

AT COMMAND MODE sp1ml hyperterminal

Posted on November 15, 2017 at 15:54ok now i got the firmware and download the binary to the sp1ml using st-link , looks it is downloaded , now i want to test the AT COMMAND mode using the hyperterminal , first let me tell you the hardware connectio...

IDW01M1 Wifi Sample Codes for STM32F411RE

Posted on April 26, 2017 at 07:24Hello!I recently bought the IDW01M1 WiFi expansion board and I am trying to have it working with the STM32F411RE.However, from the examples in en.x-cube-wifi1_firmware.zip,I can find the .bin file for STM32F401RE-Nuc...

NTP request problem on SPWF04

Posted on January 24, 2018 at 14:43Hi,I'm working on SPWF04 linked by UART with a NUCLEO F411RE board; I'm facing with a strange problem: I'm trying to connect with an NTP server to synchronize the NUCLEO RTC, so after create a wifi connection, I op...

DUrbano by Associate III
  • 5331 Views
  • 22 replies
  • 0 kudos