User Activity

Hi,I'm trying to interface this eeprom with Bluenrg2 http://ww1.microchip.com/downloads/en/DeviceDoc/Atmel-8828-SEEPROM-AT24CM02-Datasheet.pdfI can write correctly. I can read 1 byte at time correctly. Trying to read more than 1 bytes results in inco...
Hi,using the new sdk 3.0.0 I get a big increment in size of libbluenrg1_stack.a. With the same project the size jumps from 74K to 103K !Is it normal??libbluenrg1_stack.a: [15] aci_events.o 2 906 272 acl.o ...
Posted on April 09, 2018 at 15:02 Hi, I'm trying fw bluetooth update withBLE OTA service manager followingAN48 I successfully flashed theOTA_ResetManager.eww (ServiceManager workspace). When I try to flash the Ble_Beacon ( ServiceMan...
Posted on February 01, 2018 at 15:35Hi,I have a bluenrg-1 as a central and a smartphone as a peripheral. Central can connect and discovery correctly.When I try to write a pheriperal's value, aci_gatt_write_char_value() return 0x01.aci_att_prepare_wr...
Posted on January 12, 2018 at 12:33Hi,when I set the authentication requirement to SC_IS_SUPPORTED, the pairing process fails with the error: SMP_SC_DHKEY_CHECK_FAILEDWhat can I do?Thanks#bluenrg