Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-NUCLEO-IDB04A1 with Nucleo STM32F103

Posted on January 31, 2018 at 19:51Hi.I am using the  X-NUCLEO-IDB04A1 with Nucleo STM32F103 and the available demos are only for F4, L0 and L4. This is fine as I want to learn about programming bluetooth anyway. The BLUENRG chip on the expansion bo...

M Greally by Associate II
  • 1486 Views
  • 2 replies
  • 0 kudos

SPBTLE-1S Program

Posted on October 19, 2017 at 04:29Hello, Mr, Ms. I want to program SPBTLE-1S.I want to use the bluetooth module to send signal from MCU to Smartphone. To do that, do I need to program the SPBTLE-1S?How can I do that?I can not find any evaluation bo...

SPWF04S SPI basics problem

Posted on July 24, 2017 at 14:31Hi there, I have alot of problems with SPWF04S and its SPI interface. From the datasheet this is what should happen:TX:1. The communication starts with the host sending the write SYNC word (0x02), 2. followed by heade...

Observation/Discovering BLE device using BlueNRG

Posted on January 25, 2018 at 18:49I am currently trying to discover a BLE compatible device (e.g. iphone) using BlueNRG GUI (v2.6.0) and STEVAL-IDB007V1. I tried running ACI_GAP_START_OBSERVATION_PROC and ACI_GAP_START_GENERAL_DISCOVER_PROC, which ...

K C by Associate II
  • 1750 Views
  • 4 replies
  • 0 kudos

Resolved! BLE Scanning on single channel only

Posted on January 30, 2018 at 17:41Hello, I am currently working with STEVAL-IDB007V1 evaluation board along with BlueNRG GUI, to scan/debug Bluetooth device.For development purposes, I have advertisement packet broadcasting on a single channel only...

K C by Associate II
  • 2076 Views
  • 6 replies
  • 0 kudos

Disable automatic wi-fi connection on SPWF04

Posted on January 31, 2018 at 09:37Hi to all,I'm working on SPWF04 wifi module and, even I read all at possible commands, I don't find how to disable the automatic wifi connection to an access point on start-up. Please, could anyone suggest me ho do...

DUrbano by Associate III
  • 980 Views
  • 3 replies
  • 0 kudos

SPWF04 Station Disassociation

Posted on February 03, 2018 at 06:29I am using SPWF04 module for embedded web server application. I can access web pages on the web server from the PC/laptop, but when i access from android phone wifi module reports station disassociation.

SPWF04SA always return ''Hardware Failure''

Posted on August 10, 2017 at 09:47Hi ST,Recently I try to enable AP or station mode on SPWF04SA wifi module,I connect it with my PC via UART and I can see some feedback on terminal on my PC.The question is, even though I can command SPWF04SA with it...

Wei Lu by Associate
  • 923 Views
  • 1 replies
  • 0 kudos