Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Spirit1 starnge condition

Posted on November 18, 2015 at 19:31Hello everybody! Guys? I have interesting problem. When data  TX spirit1 displays the status of 0x26 and transmit non started(no event max_TX_reach), but I'm read events IRQ register before transmit, this reg. ind...

rm by Associate
  • 1333 Views
  • 3 replies
  • 0 kudos

Using aci_gap_set_undirected_connectable()

Posted on March 07, 2018 at 16:19Hello all,I am using a bluenrg-1 working as a peripheral, I get the unit paired to two devices (mobile phones) using authentication. One phone uses RANDOM address and the other one uses PUBLIC address. I can see both...

jampino by Associate III
  • 755 Views
  • 0 replies
  • 0 kudos

SPWF01SA - Error loading webserver pages

Posted on March 09, 2017 at 15:06Hi,I'm using wifi module SPWF01SA with firmware version 160129-c5bf5ce-SPWF01S.I uploaded my webserver on the wifi module, using the guidelines: /external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen...

Resolved! SPWF01: Running example applications

Posted on February 18, 2018 at 18:35Hi,I get troubles to start with my new IDW01M1 module.I use it with the NUCLEO-L053R8 board, but none of applications provided with the WiFi CubeExpansion package works with my hardware.For example, I load the 'Wi...

SPWF04SA: Where is my NTP request response?

Posted on February 22, 2018 at 22:40Hi,I'm working with SPWF04SA using UART in a custom project. I have a issue making calls to NTP server. I've tried with several servers, but the behaviour is the same, I can't get response.This is what I send and ...

Using X-NUCLEO-IDB04A1 with BlueNRG GUI fails

Posted on November 11, 2016 at 15:16HiI want to evaluate BlueNRG using the BlueNRG GUI. My setup is as follows:NUCLEO-F401RE with X-NUCLEO-IDB04A1 installed.BlueNRG GUI software version V2.2.1 (latest)X-CUBE-BLE1 Cube Expansion packageI've followed ...

phorn9 by Associate
  • 4932 Views
  • 11 replies
  • 1 kudos