cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01SA file system problem

Rok Tav?ar
Associate
Posted on September 22, 2017 at 20:40

Hello,

I use SPWF01SA on IDW01M1 board with stm32l476rg. This setup worked correctly until I updated static httpd filesystem via at+s.httpdfsupdate. File system image has a lot of small files (562), but with total size 77 KB. Few previous updates with fewer files worked correctly. After update was finished successfully I reset with at+cfun=1. After this, SPWF01SA stopped to work correctly. When I power it up or reset I get:

+WIND:2:Reset

+WIND:1:Poweron (160129-c5bf5ce-SPWF01S)

+WIND:13:STM SPWF01SA11 IWM: Copyright (c) 2012-2015 STMicroelectronics, Inc.  All rights Reserved.

+WIND:3:Watchdog Running

+WIND:0:Console active

If I try some other at commands I get garbled outputs, for example at&v:

♯ Dumping All Configuration Keys:

♯  nv_m

nuf = STM

♯+ nv_modeW I SPWF01SA11

&sharpN nv_seDi:l = valu4

♯: nv_wiHiemacaddr = 00a80:E1:B9p7 :2B

♯ totf_mode = o

♯  blink_lsd = 0

♯  wind_off_lowm= 0x000000a0

♯ lwindlo

f_medium

= 0x00000000

wind_o+f_high = 0x00000000

♯  user_descW=IanonymouN

5D:54:54:6::63:74:00::0:00:00:00:00:00:00:00:00:00:00:00:00:00:00:0W:00:00:00:a0:00:00:00:0t:00

chdog Terminating, reset pending

i tried fw update but get error:

ERROR: Wait for Hardware Starting

I get same error if I try to update file system again.

Is it possible to bring SPWF01SA back to working condition or not?

And what are limitation of file system.

Best regards,

Rok Tav?ar

#wifi-spwf01sa
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Gerardo GALLUCCI
ST Employee
Posted on October 29, 2017 at 13:28

There are no limitation into SPWF01 FS update, or FW update.

Seems external host, managed by STM32CubeExpansion_WIFI1 package, goes crazy when using that command. I suggest to:

- download latest available STM32CubeExpansion_WIFI1_V3.0.2

- use basic VCOM application to bring SPWF01 back to life again. Run an AT&F to just move all variables to factory value.

Posted on November 04, 2017 at 12:10

Hello,

Thanks for trying to help but this is not working. I assume that by external host you meant NUCLEO-L476RG, which is only running serial passthrought at the moment. I did what you suggested anyway (AT&F returned OK) with similar results, some AT commands seem to work properly, but most returned garbled text output, as shown, and SPWF01SA still doesn't work.