Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST7580 transmitter/receiver circuit question

In the ST7580 application note (AN4068) the transmitter and receiver paths are connected through a DC blocking capacitor after the output of the power amplifier. Therefore when no transmission is occurring the output of the PA should be similar to a ...

LSmit.10 by Associate
  • 711 Views
  • 0 replies
  • 0 kudos

S2-LP transceiver

I want to develop 6LOWPAN over S2-LPThis mesh network have other devices that support 6LOWPAN, different to ST microelectronic manufacturer. Could I tune S2-LP in frequency, band, modulation, etc in order to can speak/listen with other devices?Best r...

Resolved! STUSB1602 SPI interface

Hello there,I am currently analyzing the STUSB1602 chip and the P-NUCLEO-USB002 eval kit. I have come across a topic I am not fully certain about. Its the SPI interface for the BMC communication. I cannot understand either it is necessary in all appl...

BlueNRG-1 software problem

Hello.My customer has problems while testing BlueNRG-1 IC:"I can not make a simultaneous connection with several slave devices with the library from the BlueNRG-1_2 DK 3.0.0 package.After connecting to the first device, an attempt to start a new sear...