User Activity

Posted on July 12, 2018 at 16:59Hello,I have a pb with UART1 for L152RE board. I connected a sensor to my board in UART2 through a Max232 and i succeed to have information to my hyperterminal (TerraTerm). But i was not able to have information in th...
Posted on May 17, 2018 at 14:40Hello,I have a prototype where a sensor send information in RS232 to my STM32152RE board through a MAX232 to convert the signal. I plugged in my board with RX/TX on USART 2 (+5V et GND).I used CUBE MX and i only modify...
Posted on April 17, 2018 at 16:53Hello,I have a STEVAL-FKI868V1 based on a Nucleo L152RE board and i would like to connect a RS232 to my RX pin to get the information and then send it when i click on the button.So my main problem is about the code t...