Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RSSI value of a mesh network node

helloi would like to know if it is possible to get the RSSI value of a node while it is provisioned in the mesh network. i am testing with 3 steval IDB007V2 evaluation board and i want to know how to get the RSSI value of one node A in mesh network w...

FChou by Associate II
  • 2585 Views
  • 5 replies
  • 0 kudos

Can the BlueNRG-2 chip be programmed through SWD?

I have the STEVAL-IDB008V2 board, and it programs decently through the ST-Link V2. However, I am facing troubles with programming the BlueNRG-2 chip through SWD of another Disco board. Can anyone please tell me whether the BlueNRG-2 can be programmed...

abbas14 by Associate II
  • 573 Views
  • 0 replies
  • 0 kudos

Sending At Commands to SPBT3.0DP2 via mbed

I am trying to use mbed to send AT Commands to the SPBT3.0DP2 module in order to change it's baud rate. I am using the ATCmdParser to send the AT commands. It seems like I am not able to enter the command mode? I'm not sure. please help.I do at.send(...

JMin.17 by Associate II
  • 955 Views
  • 0 replies
  • 0 kudos

Error message "Could not initialize BlueNRG Mesh library!", error code = 2 when using pre-built bin file for NUCLEO-L476RG with X-NUCLEO-IDB05A1

I also built firmware from provided sources and libraries using WorkBench but the problem persisted. One thing was different, bin file was less than half the size of the pre-built one. I added some code to display returned error code (2) and also dis...

Boris3 by Associate
  • 1056 Views
  • 1 replies
  • 0 kudos