Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-1 software problem

Hello.My customer has problems while testing BlueNRG-1 IC:"I can not make a simultaneous connection with several slave devices with the library from the BlueNRG-1_2 DK 3.0.0 package.After connecting to the first device, an attempt to start a new sear...

Zigbee Smart Energy 1.2a

I would like to know if it is possible to create a device compatible with Zigbee Smart Energy 1.2a standard from the STM32WB55xx devices. I have seen the library STRF4CE for Zigbee implementation but I am not sure if it works for this version of stan...

Zartagal by Associate II
  • 1137 Views
  • 1 replies
  • 0 kudos

STWLC33 - IDE & Advices

Hi,i need to find the right IDE for programming STWLC33 in ISB042V1 Board. Is there any programming advice / code samples in the STM webworld?

roku by Associate II
  • 749 Views
  • 0 replies
  • 0 kudos

I'm starting for a PLC (power line communication ) modem design for transmission over a power line that along his activity can pass from 500 Vac to 24 Vdc or to cold status in a mesh private network .

My question is to verify if the component ST8500 can satisfy what is described previously taking into account that when it has to work with line at 24 Vdc or when in cold status it can't detect any "zero crossing" .Thank you

LPizz.12 by Associate
  • 526 Views
  • 0 replies
  • 0 kudos

Implementing sensor model with bluetooth mesh

I need to implement sensor network with bluetooth mesh having three nodes. Two nodes would be STEVAL-IDB007V1 boards and one of the node would be smartphone which is used to display sensor data from two nodes (STEVAL-IDb007V1) . It is required to col...

MH1 by Associate II
  • 2342 Views
  • 6 replies
  • 0 kudos

List of parts BLUENRG-1 balun

Hello everybody,I designed a board with Bluenrg-1 and discrete balun with the topography draw in the Datasheet.. the problem is that there isn’t a BOM with the value of passives of the balun... where Can I found it? I used the values of the balun of ...

SDK for STream plug.

Hi. I'm trying to design PCB for ST2100, but never worked with this. There is information in quick Start guide about STream plug SDK. Where can i find this?

AZayt.11 by Associate
  • 555 Views
  • 0 replies
  • 0 kudos