The VL53L1 GUI does not see the sensor.But the SimpleRanging works with the board:================================================================VL53L1X Examples...VL53L1X Model_ID: EAVL53L1X Module_Type: CCVL53L1X: EACCRanging loop startsCount= 0...
I try to make multi-connection using BLE lib from BlueNRG-1_2 DK 3.0.0.I cannot connect a second slave device to control after connecting to the first device.The aci_gap_start_general_discovery_proc() failed:0x82Discovery procedure are possible to s...
If I changed the definition LS_SOURCE=LS_SOURCE_INTERNAL_RO, the procedure DeviceConfiguration() stopped in line "while(CKGEN_BLE->CLK32K_IT == 0);"It seems that the internal generator 32 kHz does not work.How I can to turn on generator 32 kHz.