User Activity

Hi, as per datasheet of STM32F412VG all IO's are compliant (page 124) to CMOS & TTL, it's OK for input signal, but while configuring pin as output, how we will come to know logic level for the same, as VOH (min) is 2.4 for TTL & for CMOS it is (VDD-0...
what will be the maximum size of external parallel SRAM & NOR flash, that can be interfaced with STM32F429IIT6?
Hi trying to reduce the current consumption in STM8L151F2 series controller in HALT modebut unable to achieve the 0.4uA current rating as mentioned in datasheet, also want to make the automatically shift the MCU on HSC, but it is not happening, as my...
I am using STMPE811QTR in my project for touch screen detection, schematic is similar to STM32F429 discovery board (display size 800 x 480)STMPE811QTR is interfaced with STM32F429 on I2C bus, During the normal operation (if we touch the screen------i...
Kudos from