Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STKNX Linear regulator dropout

Hi,I would like the DC/DC converter of STKNX to make 5V.Also, I want the Linear regulator to make 3.3VBecause of global efficiency, I wanted to power the linear regulator with the 5V output of DC/DC converter.I'm surprised that the datasheet specifie...

potting BLUENRG-M2SP and BLUENRG-M2SA

Hello,I hope you are well.I am using your bluetooth modules with chip antenna “BLUENRG-M2SA” and PCB antenna “BLUENRG-M2SP”.I'm going to put the 2 modules in the potting ? is there an influence of potting on the characteristics (range, transmission, ...

ljm by Associate III
  • 1462 Views
  • 3 replies
  • 0 kudos

X-NUCLEO-BNRG2A1 UART Bootloader Mode

Hello, Following AN4872  & UM2667 I did the following: - Connected J15(Force DIO7 High).- UART-Connection is like(Beside GND and Vdd):    Nucleo-Board(F401RE)   <----------------------->  X-NUCLEO-BNRG2A1       PA9(UART1_Tx)           <--------------...

AElgh_0-1736432060174.png AElgh_1-1736432143666.png AElgh_3-1736432241818.png
AElgh by Associate III
  • 756 Views
  • 0 replies
  • 0 kudos

Resolved! M48T18-150PC1 Timekeeper

I have a circuit card that uses the M48T18-150PC1 Timekeeper SRAM, and the battery died. I replaced the part but the settings did not save once power was cycled. A second part was used with the same result. Looking at the date stamp, (412) tells me I...

BobW777 by Associate
  • 1585 Views
  • 2 replies
  • 1 kudos

Layer Stackup for BALF-WL-00D3

 My team is trying to design a radio board with the STM32WL and we plan to use the BALF-WL-00D3 in the RF Front End.Based on our requirements, we have decided to go with a 6-layer board and are trying to decide on a stackup (dimensions) for the same....

ST8500 FSK modulation

Hi, I am evaluating to use the ST8500 module as alternative part of the ST7538Q.In our application we have a custom protocol over power line with FSK modulation.Looking all the documentation related to ST8500 I found that it is possible to configure ...