Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2lP error code "LOW BATTERY Indicator"

I have reference H/W design by X-NUCLEO-S2915A1.It has still have "IRQ_LOW_BATT_LVL" and not send TX data.-Pin1, Pin7, Pin10, Pin15 is 3.3V Level.Could please let ms know if you have any recommend my check point...

CKim.18 by Associate II
  • 779 Views
  • 0 replies
  • 0 kudos

Resolved! Is BLUENRG-2 working in DTM mode suppose to send some HCI Command Packets to controlling host MCU ?

Hi, I'm using BLUENRG-2 chip with DTM (UART) FW as a BLE module for my STM32 processor. In general everything works - I'm able to set-up profiles, establish connection with central, send notification and receive data from characteristics. To achieve ...

Wojciech by Associate II
  • 1954 Views
  • 3 replies
  • 0 kudos

Programming spec for BLUENRG-2

Good day. This is IC programming manufacturer.We have to support this BLUENRG-248  QFN48 on our IC programmer. Could you help to provide the programming spec to us for development?Please let me know if we need to sign NDA.

JHsu.14 by Associate II
  • 774 Views
  • 0 replies
  • 0 kudos

Using KSZ8863 als Sniffer

Hello everyone,I'm trying to use a KSZ8863 to monitor ethernet traffic. the KSZ8863 is connected to a STM32F767 via RMII.Im using the STMcubeIDE lwIP stack.I have no problem getting a ip-adress and ping the STM32. Also the SMI interface to the KSZ se...

y.rr by Associate II
  • 1832 Views
  • 2 replies
  • 0 kudos

HCF4010Y CAN USE AS CMOS TO TTLCONVERTER

Hello,Iam using HCF4010 for my project. Can i use this as CMOS to TTL converter?Also for high speed switching or for high speed signal is there any issue for using the same ic(Please find the attached image,4 GPIO & 2 spi lines were used)

0690X000008ilGUQAY.jpg
AThom.17 by Associate II
  • 1149 Views
  • 2 replies
  • 0 kudos