Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I want to take images from a CMOS camera and wanna send to a mobile phone, It is clear that DCMI offers perfect solution to get images but I could not find any sufficient way to send images to a mobile phone via wireless communication.

More spesicifly , I could not calculate the data size for every image and I am not able to determine which wireless communication protocol for mobile phone suits to my project. Would you guys give me clue,reference or idea?

NUCLEO-L476RG with I-NUCLEO-LRWAN1 time out

Dear all,I have 2 NUCLEO-L476RG with 2 I-NUCLEO-LRWAN1 lora shield.I plug the shield on the nucleo, connect the antenna, connect the nucleo on my computer, and I compile and load the ping_pong demo program sx1272mb2das from "en.i-cube_lrwan" into eac...

jarjar by Associate
  • 1983 Views
  • 4 replies
  • 0 kudos

SPBTLE-RF0 Bluenrg-ms Max_Attribute_Records

Hello,I want to know about how to calculate max attribute records when I want to add server ? Is there a limitation of number of servers or characteristics ? If there is a limitation about characteristics or servers number, how many byte or number?Th...

MKara.10 by Associate
  • 630 Views
  • 0 replies
  • 0 kudos

SPIRAW Function of S2LP-SFX-DK

Please let me know the SpiRaw function data format in S2LP-SFX-DK. in_buffer [0] - 0x00 is SPI Write, 0x01 is SPI READ, 0x80 is Command in_buffer[1] - SPI Reigster Address or Command in_buffer[2]~ - Write Data

CKim.18 by Associate II
  • 1708 Views
  • 3 replies
  • 0 kudos

How to make s2lp go to TX MODE

HiI tried to develop my own code for s2lp on NUCLEO-L476RG my setup include:NUCLEO-L476RG+s2lp FKI433v2 on top(RX working fine)NUCLEO-L476RG+s2lp FKI433v2 on top(TX cant go to TX mode)NUCLEO-L053R8+s2lp FKI433v2 on top(as a test for both RX and TX)I...

0690X00000AALATQA5.png
malsh by Associate II
  • 1399 Views
  • 3 replies
  • 0 kudos

STUSB4500 datasheet VCONN pin confusion

I am designing a device using the STUSB4500 in QFN-24 package. In the datasheet, pin 3 is both specified as NC and VCONN.The pinout says it is NC, but in any example schematics, this pin is shown as VCONN.In different resources, this pin is either be...

PDobo by Associate II
  • 1232 Views
  • 3 replies
  • 0 kudos