Good day!How much time will the node work in the MESH network, if it is powered from a 3.6V battery with a capacity of 1800 mAh? It is assumed that all nodes operate in standard mode and low-power nodes in the network are not used. Transmitter power ...
I am trying to implement a working MESH network without the participation of a smartphone. The idea is to send messages from all test nodes to one specific node through the MESH, which has the same hardware structure as the rest. This node should pro...
I am trying to select smartphone for MESH activity.Please, tell recomendations for kind of BLE version for smartphone bluetooth adapter.Does either version BLE4.0 is sutable for that, or BLE5.0 and higher is only appropriate?
Martin, good afternoon!Please help with advice on how to change the background of the keyboard in this example.And one more question. Why can't I use the "keyboard widget" in the field of available widgets from the touchGFX?
Hello! I have a similar problem when using TuchGFX and ssd1963 based display. I have a custom board with a stm32f407vgt6 controller. From this FSMC links to control the display based on ssd1963 through 16bit interface. Can I use the capabilities of T...
Hi Winfred!Thanks for the answer in my topic. Hope you are well.I found that the reason for the incorrect work of the program was the discrepancy between the assignment of pins for the UART and the PWM. Sorry for my hasty questions in the past. I hop...
Hi, Winfred!Thanks for the answer. I received the correct response from the PCB using the debugger. However, there are some features. The fact is that I managed to get the correct response only in the uKeil debugger mode. I do it like this.I launch t...