Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-2 VBAT max rating

Hi,I'm designing a beacon around the BlueNRG-2 and would like to power it from a battery that can output as much as 3.67V. Unfortunately this exceeds the max Vin limit on the datasheet (3.6V) by only 70mV. I have a couple of questions in the hopes of...

jaylong by Associate II
  • 566 Views
  • 0 replies
  • 0 kudos

Question on setting for NRG-1 and NRG-2

I am using NRG-1 for my product development but I have only NRG-2 kit on hand. I am using NRG-2 project to develop my SW for using DK kit but I found there are 250kHz frequency offset when the software is applied to my HW for using NRG-1 inside. Is...

HLI.16 by Associate
  • 1174 Views
  • 4 replies
  • 0 kudos

Spectrum distortion in maximum power setting

Hi all,I am working on NRG-132 for my product development and it is fine for spectrum with Power Level from 0 - 14 (ie -18dBm -- 4dBm). However, when I set to powerlevel = 15 or PA_level in BlueNRG GUI in level 7, the output spectrum will be distort...

HLI.16 by Associate
  • 675 Views
  • 0 replies
  • 0 kudos

Balun options for BlueNRG?

I'm using BlueNRG132 (QFN32) in a custom PCB project. Currently I'm using BALF-NRG-01D3 chip, but I would like to know if there are other options of Balun Chips to use with BlueNRG and 2.4 Ghz (50 Ohm matched) antenna. On the other hand, I would like...

FHern by Associate
  • 784 Views
  • 1 replies
  • 0 kudos

How to implement resolvable and non-resolvable private addresses in the BlueNRG-2 module using Keil?

Hi, i am new to using ST boards. I am using a broadcaster which only sends data after every particular interval. I want to use resolvable and non resolvable private address techniques to secure the data sent and direct it only a particular user and n...