User Activity

Hello,thermal data of the L78M show junction-to-ambient thermal resistance (θJA) and junction-to-case thermal resistance (θJC) for different packages (e.g., TO-220 and DPAK). Those figures differ, of course. Note that the datasheet provides no juncti...
I'd like to use the ST202/ST232 as a drop in replacement for MAX202/MAX232 devices. In my design, the V+ output is connected to GND (via capacitor) as suggested in the datasheethttps://www.ti.com/lit/ds/symlink/max232.pdfWhereas the ST datasheethttps...
The ST202EB (ST202EC, ST232EB, ST202EB, ...) RS232 receiver's datasheets shows the following application circuit.Table 7 lists recommended capacitors values for C2-C5 (for the device ST202E is states 0.1 nF, for device ST232 it states 1uF).I think t...
Kudos given to