Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Where I can find the wmbus_link.c file?

Hi,  I am looking for the wmbus_link.c file, that contents in the WMBUS Library 2013. Could you please tell me where I can find this file?I have read from the document AN4772 with title ‘Wireless M-Bus link layer’, especially in the section 5.3.1- Fi...

Why the SPIRIT1 (SPSGRF 868 module) enters in MC_STATUS ERROR when I send to it via SPI the command to enter in LOCK status during the "WMBus_PhyInit(MODE, TYPE)" undebuggable initialization function?

Hello,I'm working with a custom board mounting the SPSGRF-868 RF 868MHz module, which embeds the SPIRIT1 transceiver.I communicate with it via SPI, using a microcontroller STM32L151.My board is based on the STEVAL-IDS001V4M evaluation board architect...

mikmary by Associate II
  • 1443 Views
  • 1 replies
  • 0 kudos

What is advertisement_interval_min,advertisement_interval_max, connection_interval_min and connection_interval_max in BLE terminology?

My question is with reference to the following API.aci_gap_set_discoverable(uint8_t Advertising_Type,                  uint16_t Advertising_Interval_Min,                  uint16_t Advertising_Interval_Max,                  uint8_t Own_Address_Type,  ...

Akram by Associate
  • 6831 Views
  • 3 replies
  • 0 kudos