Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Control AMIS-30543 with STM32F030R8

I'm setting up a MCU to control a stepper motor. I'm aiming to control the stepper motor driver (AMIS-30543) over SPI. My current goal is to get the driver to respond to my SPI commands so I know it's correctly receiving my commands. The driver respo...

SNeub.1 by Associate
  • 6654 Views
  • 13 replies
  • 0 kudos
BV.1 by Associate
  • 1258 Views
  • 1 replies
  • 0 kudos

We are implementing the SPBTLE-1S as an off-the-shelf BLE solution, and we can't find any documentation about the default Mode, as apparently it can operate in 4 different interface Modes: "000", "001", "100", and "010", as per the data sheet.

Ideally, I need it to work in serial1 or Mode "001" on boot.  Is this indeed the firmware default? As an integrated BLE module I would expect it to work immediately, i.e. plug and play but in which mode? I assume I can change firmware and/or registe...

tidd by Associate II
  • 2825 Views
  • 4 replies
  • 0 kudos

SPBTLE-1S DTM using UART using non-st platform

I have a board which uses the SPBTLE-1S interface via UART with an NXP I.MX RT 1060. I've downloaded the BlueNRG-2 code. I'm looking to get a DTM running on our processor. Has anybody ported the DTM example code to a non stm32 processor?At first glac...

JHade.1 by Associate
  • 674 Views
  • 0 replies
  • 0 kudos