Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why provisioning did not happen the second time, once unprovisioned the node first-time blemesh mesh app using STEVAL_IDB008V2?

Hi sir/Madam,If we flashed BlueNRG2_Lighting_Demo.bin file using USB micro in STEVAL_IDB008V2 board it was provisioned. If we give commands from models, board doesn't show any change in the led, why? So that we unprovisioned node and tried to provisi...

Anitha by Associate III
  • 907 Views
  • 0 replies
  • 0 kudos

Is BlueNRG-Tile support notifications from more then one characteristics simultaneously, if I considered BlueNRG-Tile as a client??

I am using BlueNRG-Tile chip. I am configuring it as a server. And i am using ST BLE Sensor App as a master. In that i am getting all the services and characteristics displayed on App ,which I have configured at server side. My target is to get notif...

DRamp.1 by Associate
  • 611 Views
  • 0 replies
  • 0 kudos

How can I use the LTDC on a Nucleo and wire it to my Elegoo TFT display shield (which is ILI9341, but only has 8 data pins)?

Sorry if this is a dumb question. I have a Nucleo F767ZI, and I want to wire it to this: http://www.lcdwiki.com/2.8inch_Arduino_Display.There's a tutorial here on how to set up LTDC with an ILI9341 here: http://www.lucadavidian.com/2017/10/02/stm32-u...

NNagy.1 by Senior
  • 1007 Views
  • 1 replies
  • 0 kudos

Enable disable LDC mode

Hi,I really appreciate the reactivity of the forum, thanks a lot.i have some questions:1- When i enable/disable LDC mode using S2LPTimerLdcrMode, and S2LpTimerFastRxTermTimer, i need to run command S2LPCmdStrobeReady and S2LPCmdStrobeRx after each en...

BMoha.19 by Associate II
  • 1281 Views
  • 1 replies
  • 0 kudos

BlueNRG2 - Packet Length extension (Tx direction)

using BlueNRG2, I'm trying to send long packets (> 20 bytes), I added a custom service with characteristic supporting notification and indication with a size = 40 bytes. After the connection established, I send a LL_LENGTH negotiation to update the T...

MBRAI.9 by Associate
  • 869 Views
  • 0 replies
  • 0 kudos

How to rebuilt BlueNRG-2 for UART

I need to update the pins used for UART communication by the BlueNRG-2 chip. I have found documentation that states you can update the source code as necessary. Is there any documentation on how to actually build the target .bin or .hex file after yo...

SBukh.1 by Associate II
  • 3004 Views
  • 4 replies
  • 1 kudos

STEVAL-BLUEMIC-1signal strenght

We are working with 2 STEVAL-BLUEMIC-1 boards, one configured as server and one configured as client. Server is located into a PVC box at about 2/3 meters from the client. We noticed that when we hold in hand the pvc box or when we interpose ourselve...

EBono by Associate
  • 859 Views
  • 0 replies
  • 0 kudos