cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to develop a piconet using STM32 BluenRG 2 DK by setting up one master device and multiple slave devices. Every slave is connected to an analog sensor and the master should discover the slave, connect and receive data and disconnect.

BV.1
Associate

STEMEVALIDB008 V2 is the board I am planning to use.

Link: https://www.st.com/en/evaluation-tools/steval-idb008v2.html

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Winfred LU
ST Employee

Please reference the documents in DK:

C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.1.0\Docs\Multiple_Connection_Guidelines\Multiple_Connection_Guidelines.html

C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.1.0\Docs\Multiple_Connection_Formula\Multiple_Connections_Formula.html

View solution in original post

1 REPLY 1
Winfred LU
ST Employee

Please reference the documents in DK:

C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.1.0\Docs\Multiple_Connection_Guidelines\Multiple_Connection_Guidelines.html

C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.1.0\Docs\Multiple_Connection_Formula\Multiple_Connections_Formula.html