Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why i cant read and send data between UART2 of a STM32L412RBT6 (PA2 and PA3) and the BlueNRG-M2SP UART(DIO8 and DIO11)

I designed a PCB with an STM32L412RBT6 and a BlueNRG-M2SP, and I checked the connection and I can't read data from the bluetooth module and I can't send data from the STM32.I made the following code:stm32l4xx_it.cvoid USART2_IRQHandler(void) { /* U...

0693W00000KcGmRQAV.png
PCong.1 by Associate II
  • 3062 Views
  • 6 replies
  • 0 kudos

Resolved! STUSB4700/4710 I2C register details

I am working on a project using a few STUSB4710 and some STM32F0 family microcontrollers. I am looking for details about the registers of the STUSB4710. In the datasheet I can find only the I2C register map and the details of the PDO registers but no...

Buffer error after debug in the variable field there is an error message uint8_t buff_tx[10] = {11,12,13,14,15,16,17,18,19,20}; program was taken from you tube link : https://www.youtube.com/watch?v=xE6GVt7XuJI

buff_tx Error: Multiple errors reported.\ Failed to execute MI command: -var-create - * buff_tx Error message from debugger back end: -var-create: unable to create variable object\ Failed to execute MI command: -var-create - * buff_tx Error message ...

RKore.1 by Associate II
  • 1390 Views
  • 3 replies
  • 0 kudos

Operate Teseo-Liv3F module in standby mode

Hi team,We have a snapdragon 820 based board running with debian OS(linux kernel-4.14). we have interfaced Teseo-LIV3F to the Snapdragon 820 over the UART and using gpsmon application to read latitude and longitude valuescommand used,$ gpsmon /dev/tt...

Deepika by Associate
  • 787 Views
  • 0 replies
  • 0 kudos