2021-10-29 5:07 AM
Hello,
I would to access to i2c devices with bluenrg-355MT, I use functions from BlueNRG-LP DK 1.0.0, in bluenrg_lp_evb_i2c files. When I Download and Debug, i2c works fine, but in release mode there is no i2c signals.
Here my code to detect light sensor :
BSP_I2C_Init();
HAL_StatusTypeDef ret;
ret = HAL_I2C_IsDeviceReady(&hi2cx, 0x10<<1, 1, 10);
if( ret != HAL_OK )
printf("Device not present.\r\n");
else
printf("Light sensor detected.\r\n");Whatever the parameters, there is no signals.
I2C is configured like this :
/* Initialize the GPIOs associated to the I2C port */
BSP_I2C_DATA_GPIO_CLK_ENABLE();
LL_GPIO_SetPinMode(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetPinSpeed(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_SPEED_FREQ_HIGH);
LL_GPIO_SetPinOutputType(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
LL_GPIO_SetPinPull(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, BSP_I2C_DATA_GPIO_PULL);
BSP_I2C_DATA_GPIO_AF();
BSP_I2C_CLK_GPIO_CLK_ENABLE();
LL_GPIO_SetPinMode(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetPinSpeed(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_SPEED_FREQ_HIGH);
LL_GPIO_SetPinOutputType(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
LL_GPIO_SetPinPull(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, BSP_I2C_CLK_GPIO_PULL);
BSP_I2C_CLK_GPIO_AF();
/* Initialize the I2C clock */
BSP_I2C_CLK_ENABLE();
LL_I2C_Disable(BSP_I2C);
/* Configure the SDA setup, hold time and the SCL high, low period
* For Fast-mode 400 kHz, PRESC | 0h | SCLDEL | SDADEL | SCLH | SCLL
* 1h | 0h | 3h | 2h | 03h | 09h
*/
LL_I2C_SetTiming(BSP_I2C, 0x10320309);
/* Enable Clock stretching */
LL_I2C_EnableClockStretching(BSP_I2C);
/* Enable Peripheral in I2C mode */
LL_I2C_SetMode(BSP_I2C, LL_I2C_MODE_I2C);
/* Enable the I2C peripheral */
LL_I2C_Enable(BSP_I2C);Its I2C1 CLK-PA0 DATA-PA1
Could debug mode force peripheral to work by enabling all clocks and power paths, so i forgot to enable something ? Or what the difference between release and debug in µC configuration point of view ?
Thanks for any help,
Andy.
Solved! Go to Solution.
2021-10-29 6:06 AM
Hi @Community member ,
I guess this behavior is linked to PA0 and PA1. LEt me share my hypothesis here.
I suppose you are using ST-Link as debug/flash probe.
In fact, PA0 and PA1 are also JTAG pins.
ST-Link probe is sending a specific sequence leading to reconfiguration of PA1/PA0 for JTAG.
Unfortunately, this JTAG configuration can be cleaned only by a PowerOnReset. A HW_Reset does not affect JTAG config explaining behavior you noticed.
After flashing, if you perform a power on reset ( power off on your board), your I2C should be functional as per what you see in debug mode.
This specific sequence of SWD-to-JTAG is present at the end of any ST-Link operation such as debugging or also programming.
Only a power On sequence can erase JTAG configuration ...so a power on reset to restart the application is needed.
I know that this is very annoying to do power off and power on. So, in this case, I suggest to use another debugger as solution.
I could advise usage of the CMSIS DAP debugger as per default probe use on BlueNRG-LP eval board : STEVAL-IDB011V1 board.
FYI, you could try to get this one (of course it exists other references)
www.electrodragon.com/product/daplink-cmsis-dap-debugger-arm-cortex-stm32-mdk
You can also flash your binary using UART bootloader.
Regards,
Sebastien.
2021-10-29 6:06 AM
Hi @Community member ,
I guess this behavior is linked to PA0 and PA1. LEt me share my hypothesis here.
I suppose you are using ST-Link as debug/flash probe.
In fact, PA0 and PA1 are also JTAG pins.
ST-Link probe is sending a specific sequence leading to reconfiguration of PA1/PA0 for JTAG.
Unfortunately, this JTAG configuration can be cleaned only by a PowerOnReset. A HW_Reset does not affect JTAG config explaining behavior you noticed.
After flashing, if you perform a power on reset ( power off on your board), your I2C should be functional as per what you see in debug mode.
This specific sequence of SWD-to-JTAG is present at the end of any ST-Link operation such as debugging or also programming.
Only a power On sequence can erase JTAG configuration ...so a power on reset to restart the application is needed.
I know that this is very annoying to do power off and power on. So, in this case, I suggest to use another debugger as solution.
I could advise usage of the CMSIS DAP debugger as per default probe use on BlueNRG-LP eval board : STEVAL-IDB011V1 board.
FYI, you could try to get this one (of course it exists other references)
www.electrodragon.com/product/daplink-cmsis-dap-debugger-arm-cortex-stm32-mdk
You can also flash your binary using UART bootloader.
Regards,
Sebastien.
2021-10-29 6:34 AM
Hello @Sebastien DENOUAL ,
Nice hypothesis, thank you very much. Indeed it works after power reset or after programming with UART bootloader. I guess there won't be this issue with an OTA manager.
Thanks,
Andy.
2021-10-29 6:38 AM
Hi @Community member ,
You're welcome.
I confirm no issue while using OTA manger - This JTAG config happens only while flashing using external ST-Link probe.
Regards,
Sebastien.