cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a possibility to power off the Murata Type ABZ module completely, and remember the settings for next power on ? Like for the RN2483 ?

Loïc
Associate II

Hello everyone,

I use the Murata Type ABZ module as an AT Slave device from a bigger microcontroller. As the Murata module is one among many modules on my board, I have included the possibility to turn it off completely with a load switch. Rather than putting it into sleeping mode, could that be also an option ? If so, what would be required to do ? Which parameters should be saved ?

Thanks and best regards,

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0