cancel
Showing results for 
Search instead for 
Did you mean: 

w

MDoc.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
LCord.1
Associate III

Same I even get "WrMulti failed to send 32768 bytes to regsiter 0x00" (32768 is 0x8000 why would you send 32kibyte?) when I use get_set_params sketch.

I get "Beginning transmission to 14; Writing 1 bytes to register 0x7FFF

Write Status: 2

" twice and then "VL53L5CX not detected at requested address" if I use ranging_basic sketch. Hope somebody can beak it down. Thanks in advance

Edit: I use the ESP32 and maybe that is the cause I'll be using an arduino to test it. 

MDoc.1
Associate II

In my case, I didn't get any error except that if i dont disable the _vl53l5cx_poll_for_answer() function, the system freezes due to the do while loop inside the function, the device does not respond. I guess it has something to do with my WrMulti function.

Any update on this?

Did the Arduino work?