Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use BlueNRG GUI v4.2.0

i am not able to connect to hardware on above mention software also get the error as shown in image .i have also followed the UM2058 for steps but after following the step i am not able to connect to hardware.@Sebastien DENOUAL​ @Salvo​ @Salvatore DI...

0693W00000LwfJdQAJ.png

BlueNRG-LP DK SW issue with power management drivers causing high current draw after exiting DEEPSTOP mode

I'm using the BlueNRG-LP DK SW package to work on a STEVAL-IDB011V1 dev kit. I'm testing the HAL power management drivers.The problem I'm having is using HAL_PWR_MNGR_Request() to enter deepstop mode (which is called POWER_SAVE_LEVEL_STOP_WITH_TIMER...

Jerrold1 by Associate II
  • 1001 Views
  • 0 replies
  • 0 kudos

Resolved! How to update BLE sensor demo example code value

Hi @Sebastien DENOUAL​ ​ I have example code BLE sensor demo in that they have 3 sensor value and one free fall characteristics. One is acceleration , temp, press, and free fall. The acceleration sensor value is Conntiniously updating over the app on...

Resolved! BlueNRG-LP Extended Broadcast

Hello, I'm trying to program a STEVAL-IDB011V1 board for a broadcast role with extended advertising and Coded PHY. But something is wrong in my GAP set configuration because when I run my program I got this status from aci_gap_set_advertising_config...

DLoza.2 by Associate III
  • 2166 Views
  • 7 replies
  • 0 kudos