2021-11-25 3:25 AM
Hello everyone,
I have in my possession a X-NUCLEO-BNRG2A1, in order to get familiar with BlueNRG-M2SP. After using and tweaking STM32 samples, I can use the BlueNRG-M2SP (through the expansion board) effectively. However, I saw that you can download different firmware on the BlueNRG-M2SP module, depending on the desired use.
In case I order ,lets say 20 BlueNRG-M2SP modules, will they come preloaded with a specific firmware, or do I have to programm each one separately ? And if they do come preloaded, which firmware is the "default" one ?
Thank you in advance
Solved! Go to Solution.
2021-11-26 4:49 AM
Hi @path321 ,
Let me confirm that BlueNRG-M2SP module are delivered "empty". There is no preflashed fw inside, so you have to flash needed fw.
Exception in on X-NUCLEO-BNRG2A1 where this module is available and preflashed with DTM image (network processor) .
Regards,
Sebastien
2021-11-26 4:49 AM
Hi @path321 ,
Let me confirm that BlueNRG-M2SP module are delivered "empty". There is no preflashed fw inside, so you have to flash needed fw.
Exception in on X-NUCLEO-BNRG2A1 where this module is available and preflashed with DTM image (network processor) .
Regards,
Sebastien
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.