Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using BlueNRG-LP as BlueNRG-2

Hello everyone,I recently successfully used a BlueNRG-2 chip for a BLE project (connected to an external microcontroller and integrating the BlueNRG-2 API by means of .ioc project manager). However, it needed a very small baloon which has been a real...

Problem with flashing firmware using BlueNRG GUI

i use stm32f030 with bluenrg-1 on a card i made i want to test and communicate with it using the BlueNRG GUI --------------------------------------------------------------------------------------------------------------------------But I have problems...

0693W00000QKD8vQAH.png 0693W00000QKD8lQAH.png 0693W00000QKD8bQAH.png
Aalna.1 by Associate II
  • 1444 Views
  • 1 replies
  • 0 kudos

Resolved! What additional fees / Bluetooth SIG fees apply to any development I do with BlueNRG-355MC SOC?

I am hoping this has a simple answer. If I develop a solution based on the BLUENRG-355MC and attribute that design is based STMicroelectronics SOC solution, are there additional fees I need to be aware of? I checked the following link:https://www...

JWill.8 by Associate III
  • 2698 Views
  • 2 replies
  • 0 kudos

Resolved! I'm trying to use the STMicroelectronics.X-CUBE-BLE2 version 3.2.2 to test my BLUENRG-232N device. But the mcu goes into the Infinite_Loop: during the call of the MX_BlueNRG_2_Init function

I'm working on a new IOT device. I'm using your BLUENRG-232N device with STM32L496AGI6 microcontroller, and I'm using your STMicroelectronics.X-CUBE-BLE2 version 3.2.2 stack for the firmware and the application. but unfortunately the mcu goes into th...

LAmen.1 by Associate
  • 2178 Views
  • 2 replies
  • 0 kudos

reference example project for x-nucleo-IDB05A2

Hi I am looking to used X-Nucleo-IDB05A2 board for BLE development.After reading about the information provided on the board page the only example project folder I got, i.e en.x-cube-ble2After going through all the project given in the folder I didn'...

Skada.3 by Associate III
  • 2554 Views
  • 7 replies
  • 0 kudos