STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PDM 2 PCM DMA buffer size confusion

Hello,I have a PDM MEMS microphone that I am reading in I2S master receive mode. I am trying to take this data and put it in a FIFO buffer and then output the data over UART using DMA. I must be confusing the buffer sizes because I get mostly zeros...

kcire L. by Associate III
  • 255 Views
  • 0 replies
  • 0 kudos

How to enable pdm2pcm middleware?

STM32F4-DISCOVERY board: I need to read from the mic (MP45DT02) and I was trying to use the STM32CubeIDE to generate the initialization and I cannot get to enable the pdm2pcm middleware. I have tried to configure I2S2 (no errors) but still pcm2pcm is...

RLecu by Associate II
  • 757 Views
  • 4 replies
  • 2 kudos

STM32F0 USB Audio Record

Is there any working example to do USB Audio Recording using the STM32F0? I need to send audio received by the I2S port on the STM32F0 and send it out to the host PC via USB. I have seen AN4711 and also have the Record working on the F7 with the hel...

EThur.1 by Associate
  • 324 Views
  • 0 replies
  • 0 kudos

Bidirectional i2s using SAI on stm32f4 and f7

I've got an audio codec chip with bidirectional i2s interface, but I can't find any examples or any other info on configuring bidirectional i2s through SAI and HAL in stm32 microcontrollers. I am able to configure single-direction i2s just fine. How ...

WJabl.1 by Associate
  • 240 Views
  • 0 replies
  • 1 kudos

Audio data RF synchronization

Hello,I am sampling audio data with sampling rate 16 kHz and then send it using RF to the other MCU which is sending to DAC samples with the same 16 kHz sampling rate, Im using DMA for sending data through I2S to external DAC. The problem is that the...

KD�?b by Associate II
  • 252 Views
  • 0 replies
  • 0 kudos

I2S_CKIN Not Displaying in SAI UI

Hi there!When I set up a fresh project for the STM32G431KB in STM32CubeIDE, let's say I want the SAI to be clocked by an external clock source.So, in the prefs, I set Audio Clock Input (I2S_CKIN):Then I set up my Clock Configuration:Now one would exp...

0693W000001cc9aQAA.jpg 0693W000001ccA9QAI.jpg 0693W000001cc3yQAA.jpg 0693W000001ccBvQAI.jpg
etheory by Senior
  • 257 Views
  • 1 replies
  • 0 kudos