Does the USB Audio host class on STM32F105/STM32F4 can transfer the audio from I2S input to USB Audio output?
Does the USB Audio host class on STM32F105/STM32F4 can transfer the audio from I2S input to USB Audio output?
Does the USB Audio host class on STM32F105/STM32F4 can transfer the audio from I2S input to USB Audio output?
Hi, how do i send data to the CS43L22 codec on the board? In the audio example, it sends 16bit uint values with the eval_audio_play, but on the HAL_SAI_transmit functions i can only send 8bit values. I cannot find a solution, i configured the DAC and...
Hallo, I cannot find any guideline on how to use the I2S and USB peripheral in order to interface PCs and Mac to I2C D/A and A/D converters. Talking about USB asynchronous with speeds up to 384LB/s. These boards are nowadays designed with specialise...
Posted on September 03, 2017 at 08:50 Hello, I use I2S interface on STM32F446 to read audio stream in slave mode. The master transmits MCLK, BCLK, DATA and WS signals. At the beginning everything works fine. At random point in time the strea...
Hello ST community,I am looking at the official ST example from en.stsw-stm32062_F2\STM32F2xx_StdPeriph_Lib_V1.1.0\Project\STM32F2xx_StdPeriph_Examples\I2S\Audioand the file audio_sample.c which has been extracted from here : https://archive.org/down...
Hi guys,I have an STM32F412 discovery board and am attempting to find the best solution for connecting 8xPDM microphones in 4xStereo pairs and writing the resulting WAV to USB. The method I'm currently attempting is:Use 4xI2S peripherals, each with 2...
Hi i have a Quad Ana log-to-Digital Converter (ADC)(ADAU1978). I have to interface the same with STM32F407 discovery board by using I2C. The output of the ADAU1978 quad ADC is in I2S mode . Now i want to store the I2S output data into SD card. How do...
Posted on March 30, 2018 at 08:08I have a project generated by &sharpSTM32CubeMX 4.25.0 using firmware STM32Cube FW_F4 V1.21.0. The clock configuration can be found in the attached picture below. When I debugged the generated code I have seen that ...
Posted on February 15, 2018 at 11:24I'm using stm32f217 controller for my project where i have to interface with tlv320aic1106(pcm audio codec), which requires mclk of 2.048 Mhz and a pcmSync signal of 8khz,But when I tried configuring the i2s modul...
Posted on December 04, 2017 at 04:21Hi, I am working on a project that needs to read audio signal from 4 PDM microphones. I checked that STM32F405 chipset has 2 muxed full-duplex I2S. Is that mean I can read 4 channel audio data with this mcu? Is th...