STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! connect problem - no response at all

Using STM32_Programmer_CLI.exe (v2.13.0, on Win10) I try to connect via ST-Link / SWD, It works perfectly in the GUI but if I trySTM32_Programmer_CLI --connect port=SWD ap=1nothing happens, not even an error, it just terminates. I can even write nons...

stryga by Associate III
  • 2028 Views
  • 2 replies
  • 1 kudos

SFI Via HSM

Hello Everyone,With STM32HSM -V2AE - 25-> Flashed the firmware version1.0  for 10 numbers and will the remaining 15 counts supports to flash the updated firmware version 2.0?-> If the firmware upgrade happened in field how does HSM support in that ca...

Surya S by Associate II
  • 1337 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeProgrammer v2.6.0 not supporting STLINKV3-MINIE

I am using STM32CubeProgrammer v2.6.0 with STLINKV3-SET and STLINKV2 without any trouble.   I have recently bought some STLINKV3-MINIE debug/programming probes but STM32CubeProgrammer does consider it "too recent" and I can not use them. I can not pr...

acsatue_0-1706123880469.png
acsatue by Associate II
  • 1900 Views
  • 1 replies
  • 0 kudos

Resolved! I cannot connect ST-LINK/V2

I created a new board using STM32L431CBT6. The initial programming of the board was successful. However, once a program was written, I found that it couldn't be modified again. I suspected it might be related to Boot settings, so I tried changing Boo...

pic1.jpg pic2.jpg pic3-2.jpg pic3-3.jpg
YIshi.1 by Associate II
  • 10111 Views
  • 4 replies
  • 1 kudos

Resolved! rs485 half-duplex bootloader

I have an RS585 1/2 duplex transceiver hooked to USART2 configured for hardware flow control (RS485) on an STM32L412 micro.Is it possible to program a virgin part using the STM32CubeProgrammer, and to later do a firmware update over this comm channel...

FStra.9 by Associate III
  • 7676 Views
  • 10 replies
  • 1 kudos

Resolved! STM32 system bootloader UART protocol

I am developing a custom bootloader for a client on an STM32 system. I am using STM32CubeProgrammer to exercise the new bootloader and the built-in system bootloader to investigate the protocol being used over UART. In addition, I am referring to AN ...

SidPrice by Associate III
  • 2515 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer USB programming failed

I'm using a STM32F105 and can program the firmware with an ST-Link to get firmware with USB DFU device driver on the device.The device gets recognised if I connect it with USB and I can connect and read the memory without issues.If I try to program a...

Scherm­afbeelding 2023-12-19 om 11.49.26.png
MEige.1 by Associate III
  • 8961 Views
  • 14 replies
  • 0 kudos