STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Deadlock on STM32H745I-Disco board and it Throws error "No STM32 target Found" in STM32CubeProgrammer

Deadlock on STM32H745I-Disco board .The STM32H745I-Disco board Throws error "No STM32 target Found" in STM32CubeProgrammer . Can we recover this Board if the TAG connector is connected to SEGGER DEBUG Adapter 11:10:20 : STM32CubeProgrammer API v2.5.0...

0693W000004JZZjQAO.png

I am not able to start STM32CubeProgrammer even installed Oracle JDK 13.0.1 and openjfx. What's the problem?

I am not able to start STM32CubeProgrammer even installed Oracle JDK 13.0.1 and openjfx:System: Ubuntu 18.04 VirtualBox on MacOS 10.15: ~$ STM32CubeProgrammerError: Could not find or load main class com.st.app.MainCaused by: java.lang.NoClassDefFound...

JasonZ by Associate II
  • 4049 Views
  • 8 replies
  • 1 kudos

Why it is fail to program using st-link-v2 with stm32cubeprogrammer MCU family STM32F09x/F030xc using SWD port

17:23:22 : Address : 0x00000224 17:23:22 : Erasing memory corresponding to segment 0:17:23:22 : Erasing memory corresponding to segment 1:17:23:22 : Erasing internal memory sector 017:23:22 : Erasing memory corresponding to segment 2:17:23:22 : Erasi...

CCai.1 by Associate
  • 1606 Views
  • 3 replies
  • 0 kudos

Resolved! Installintg CubeProgrammer (java issue)

Hello,I am running new windows 10 fresh install on my laptop, having issue installing BOTH CubeMX AND Cubeprog, either one of them does not launch or install or the other one does not install or launch.If I go with java OpenJDK 8, the Cubeprog works ...

0693W000004JBNZQA4.jpg
LBeau.1 by Associate III
  • 3026 Views
  • 5 replies
  • 0 kudos