STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Store data in internal flash using stm32g0x

Hi Team,I am using stm32g0x mcu to store the default chunk of data in to internal specific location for our data storage. Once it reboot it should read the default data.I tried with different mcu calls which will not synchronize with our platform.Ple...

Akuma.6 by Associate III
  • 1809 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeProgrammer Failure

Hello,The latest STM32CubeProgrammer (V 2.15.0) appears to be unable to program an STM32L471 microcontroller.It communicates successfully but fails with error:    Error: Operation exceeds memory limits    Error: failed to erase memoryThe hex file mem...

STM32 Cube PRG Fail.PNG
Chris21 by Senior III
  • 4043 Views
  • 3 replies
  • 3 kudos

No STM32 target found

Hi, I have been recently trying to leave my shallow nucleo side of the pool behind and swim towards the deeper end of the pool. But I feel like I'm drowning a bit and could use a lifeline... (:I have so far managed to connect to and write to, a small...

EOBD_1-1707333154936.png EOBD_2-1707334689895.jpeg
EOBD by Associate II
  • 4229 Views
  • 6 replies
  • 7 kudos

stlink info unknown device

I'm using the board SPIN3202. When but I can't flash. When acces to stlink info it displaysFound 1 stlink programmers version:  V2J39S27 serial:   0670FF545551677867033851 flash:   0 (pagesize: 0) sram:    0 chipid:   0x0000 descr:   unknown deviceAn...

CChav.1 by Associate
  • 3581 Views
  • 3 replies
  • 0 kudos

STMCubeProgrammer BACKUPSRAM

Hello,STM32 target : STM32H755Is it possible to see the content of BACKUPSRAM with STMCubeProgrammer?I created a project storing data at 0x38800000. The data is stored.but STMCubeProgrammer doesn't show the values stored. Regards,  

GPHIL.1 by Associate II
  • 1130 Views
  • 0 replies
  • 0 kudos

Resolved! Bug writing to FLASH with the CLI

I've noticed what seems to be a bug when writing to flash with the '-w32' flag using STM32_Programmer_CLI. My order of operations is:I erase sector 0 of the flashI read the first 8 words of Flash and verified that it's erased.I write some words to fl...

DWalk.3 by Associate III
  • 4590 Views
  • 5 replies
  • 5 kudos