STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STLink V3 Error

Hello, I use the original StLink V3 set, along with STM32CubeProgrammer via cmd. Sometimes I encounter an error where ST-Link jumps into Error: ST-LINK error (DEV_USB_COMM_ERR).I don't know how to resolve it. The only solution that works for me is to...

JJRR by Senior
  • 5446 Views
  • 8 replies
  • 1 kudos

STM32CubeProgrammer External Loader issue

I am reading a large external memory and it takes several minutes (slow bit banging SPI). To dump it to a file I have to read the memory twice because when I select "Save As" CubeProgrammer reads the default memory size (0x400) (not the 0x800000 I en...

pmachura by Associate
  • 995 Views
  • 0 replies
  • 1 kudos

STM32CubeProgramcı

Gaggiuino projesine ait "SetupSTM32CubeProgrammer_win64" programı Hp Victus Windows 11pro bilgisayarıma yüklenemiyor. Son adımda kalır (adım 8/9).EN: The programme "SetupSTM32CubeProgrammer_win64" of the Gaggiuino project cannot be installed on my Hp...

STM32CubeProgrammer 2.15.0 released

STM32CubeProgrammer v2.15.0 release informationNew features:• Added the NOR flash memory and OTP fuse programming via USB and UART using OpenBootloader for the STM32MP13xx microprocessors• Added the support for the PMIC programming via UART for the S...

Resolved! ERORR NOT FOUND

After installing the programmer to the system and connecting it to STLINK, I encountered this NOT FOUND error. I don't know where the problem is. Also, my programmer is STLINK_V2.My second question is, when I try to install the STLINK UNITY software,...

MAHDI2 by Associate
  • 2873 Views
  • 4 replies
  • 1 kudos

STLINK-V3MINIE not recognized by Windows 10

HI,  We have designed a test fixture for a 6 panel PCB in which we use 6 individual STM programmers (STLINK-V3MINIE) and we sometimes see a problem where windows no longer recognizes one of the programmers and we can't get it back (complete system re...

RBerk.1 by Associate III
  • 1172 Views
  • 0 replies
  • 0 kudos

Resolved! Unable to erase using STM32_Programmer_CLI.exe

I am trying to erase my STM32U575 which is on a Nucleo board (U575ZI-Q) and it connected to the computer via ST-Link V3. I can erase the chip fine using the GUI STM32CubeProgrammer, but the command line method does nothing. This is the output I get w...

bpat by Associate II
  • 2512 Views
  • 4 replies
  • 1 kudos