STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer and CLI cannot unlock device

I'm using a custom board for the STM32F070 device. I can't seem to connect to the USB DFU due to the device being in read protect level 1. I've verified that it is not in level 1, but actually level 0, using the ST-Link Utility and Cube Programmer vi...

TCouvrette_4-1708056325585.png TCouvrette_5-1708056354333.png TCouvrette_0-1708056101847.png TCouvrette_1-1708056200448.png

Resolved! BOOT0/NRST control with DTR/RTS

Is it possible to use the DTR/RTS pins of a UART bridge (such as FT232RL) to automate entering the bootloader in system memory for flashing firmware using STM32CubeProgrammer? Has anybody achieved this?

jefflongo by Associate III
  • 12184 Views
  • 12 replies
  • 1 kudos

Resolved! STM32H753I-Eval2 in DFU mode

Hello,I'm curious if I am going through the correct procedure to put th H753I eval board in DFU mode. I have the power jumper JP10 on PSU. I then put a jumper on JP3 which is labeled BL_BOOT0 (which as far as I know puts the H7 in DFU mode when pulle...

TLuke.2 by Associate II
  • 9624 Views
  • 11 replies
  • 2 kudos

STM32H743 External loader problem

Hello,I'm learning STM32 and wrote an quadspi external loader for my NUCLEO -144 (STM32743ZI) and 1M external flash. I've it tested in the Cube IDE and everything looks OK, I can read and write the external flash. When I use the loader in STM32Cude...

YGU.1 by Associate II
  • 19961 Views
  • 19 replies
  • 0 kudos

Firmware Update

We have implemented a custom tool, which transfers a hex firmware file via USB DFU protocol to the control. While testing we had several problems sending the firmware to the control.First we extract the memory model out of the descriptor infromations...

Tedico by Associate II
  • 7299 Views
  • 2 replies
  • 1 kudos

Resolved! ST-LINK,Programmer error:DEV_TARGET_CMD_ERR

helloI used ST link to connect to stm32H743 and reported an error during the Programmer download process:"Error:ST-LINK error(DEV_TARGET_CMD_ERR)“.But,I used j-link to connect to stm32H743 and there were no errors during the stm32IDE download process...

jack-uni by Associate
  • 5258 Views
  • 3 replies
  • 2 kudos