cancel
Showing results for 
Search instead for 
Did you mean: 

STMCube IDE: View generated run command in console

videojames
Associate III

Hello,

I am troubleshooting an issue with a provisioning and testing script using the STM32_Programmer_CLI. I get "Failed to erase memory errors" in the CLI but running (as far as I can tell) the same options in CubeIDE does not generate the same error.

It would be very helpful if I could see the CLI command in full when I run or debug on CubeIDE.

Is there such a method for doing so?

Thankyou

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Javier1
Principal

you should elavorate a bit more, what about including your script for us to see?

hit me up in https://www.linkedin.com/in/javiermu%C3%B1oz/