STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Program loading is failed

Hey Team, I am working on STM32H745 for display project.I have faced following issue. Some time when I was program my device it was completed in 1.38 minutes usually it takes around 4 minutes because of external flash erase and program loading. 1) Is...

APate.18 by Associate III
  • 2266 Views
  • 5 replies
  • 0 kudos

Resolved! ST-link V2 Connection error.

How do I solve this error? "Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication"I use SWD. I made the cable for SWD communication. The cable is connecting ST-LINK V2 between...

KimJeBu by Associate II
  • 30644 Views
  • 24 replies
  • 4 kudos

Resolved! Duplicate stm32f405rgt6

Hi, i was wondering if it is possible to make an exact copy of an existing STM32F405RGT6 and write to another. The use case for this is an open source motor controller (VESC). i have a fully functional board, and one that i have replaced the stm32 on...

Unable to boot from BANK2

Hi, I am new to STM32G4 series. I am implementing dual bank firmware update on STM32G473 custom board. I've prepared two identical bin files(compiled to 0x08000000), and flashed them to 0x08000000 and 0x08040000.With options bytes:BFB2=0nBOOT0=1nBOOT...

THsu.1 by Associate II
  • 4947 Views
  • 8 replies
  • 0 kudos

Resolved! Force hard fault

Hello,I have a project where one of the requirements is to activate the iwdt in some defined circumstances, and refresh it in other circumstances also defined. I need to collect evidence of the correct implementation of iwdt in such a way that the ac...

Cube Prog API Error write memory

Hello,I am using the CubeProgrammerAPI.dll in a C# software and I get this error : CUBEPROGRAMMER_ERROR_WRITE_MEM when I use the download function. I dont think it is a path related issueAny ideas where this problem comes from / how to solve it ?Her...

Resolved! start CubeProgrammer CLI from a custom folder path

Hi,I'm working on download an ".elf" file on MCU without using the CUBE Programmer Application.I need to start the "STM32_Programmer_CLI.exe" from any folder path, other then the default:C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgramm...

DAUSILI by Associate III
  • 4012 Views
  • 4 replies
  • 0 kudos